ATV930 drive is getting an Embedded Ethernet Comms failure when connected to the Ethernet IP network.
Issue:
What is an Embedded Ethernet Error on an ATV900 series drive?  Customer is using Ethernet IP communication.

Product Line:
Altivar 900
ATV930
ATV960
ATV980

Environment:
Embedded Ethernet

Cause:
The RSTP function is enabled by default and it not accessible from the HMI

Resolution:
Look at the attachment.

Schneider Electric Việt Nam

Phần đính kèm
Capture.PNG.png [37.46 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: