What is the pin assignment for the Profibus connections of VW3A3607 module used with Lexium32M ?

Article available in these languages: Tiếng Tây Ban Nha

The pin assignment for the Profibus connections to VW3A3607 is as follows.

Pin 3 = RxD / TxD - P   Data wire B    (commonly used color is red)
Pin 8 = RxD / TxD - N   Data wire A    (commonly used color is green)

Attached you will find an example wiring diagram.


If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-266-8705 – Option 1 or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Phần đính kèm

Profibus connections to VW3A3607.jpgProfibus connections to VW3A3607.jpg [30.61 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: