What is the part number for the CanOpen Fieldbus Option Module for the Altivar Process Drive?

Issue:
Part numbers for CanOpen Fieldbus Option Module for the Altivar Process Drive.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
VW3A3608 - 2 RJ45 Connectors
VW3A3618 - 1 x 9-way male SUB-D Connector
VW3A3628 - 1 x 5-way screw terminal block

Link to the ATV600 CANopen manual: https://www.se.com/us/en/download/document/EAV64333/
Link to the ATV900 CANopen manual: https://www.se.com/us/en/download/document/NHA80945/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: