undefined [object Object]
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
What are the default serial port settings in PM2225 meter ?
The meter is factory-configured with the following default serial communications
settings:

• Protocol = Modbus RTU
• Address = 1
• Baud rate = 19200
• Parity = Even

You can use a communications converter (USB to RS-485 or RS-232 to RS-485)
device to connect to the meter.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: