Which display settings are available on PM2225 meter display ?
Following display settings are available using the meter display:

Parameter                   Values                                   Description
Contrast                       1 - 9                      Increase or decrease the value to increase or decrease
the display contrast.

Bcklght Timeout(min)    0 - 60                  Set how long (in minutes) before the backlight turns off
after a period of inactivity. Setting this to “0” disables the
backlight timeout feature (i.e., backlight is always on).

Screen Timeout(min)     0 - 60                  Set how long (in minutes) before the screen turns off
after a period of inactivity. Setting this to “0” disables the
screen timeout feature (i.e., display is always on).

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: