How do I setup an ATV212 Drive to start and stop from face display and speed up using an external potentiometer?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
ATV212 configuration to start and stop from face display and speed up using an external potentiometer?

Product Line:
Altivar 212

Environment:
All

Cause:
Wiring and programming

Resolution:
Wiring for potentiometer:
PP for +10VDC
VIB for signal.
CC for common connection

Programming:
Mode and arrow under AUF.
Set CNOD to 1 for main front display start and stop.
Set FNOD to 2 for 0-10VDC from VIB and CC.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: