What is the maximum depth of the NetShelter SX vertical mounting rails, with or without the accessory mounting rails installed?
Issue:
Installation requires knowledge of how deep the mounting rails can go, with or without the accessory rails installed.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
Compatibility requires rail depth specification.

Resolution:

see attached

Schneider Electric Việt Nam

Phần đính kèm
Copy of Rack PMA min-max.xlsx [12.14 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: