ATS46 soft starter is blowing control power fuses on power up.
Issue:
Blowing control power fuses on ATS46 power up.

Product Line:
ATS46

Environment:
All

Cause:
NA

Resolution:
The soft starter is obsolete and repair parts are limited or obsolete.

There could be an issue with the transformer and/or cooling fan in the soft starter.

Suggested sending the soft starter in to the repair depot or replace the ATS46 with the the ATS48 soft starter.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: