What is the Schneider Electric Equivalent for PFXSP5500xxx and PFXSP5xxx?
Issue:
Looking for a cross-reference for a Pro-Face HMI with Model Number PFXSP5500xxx and PFXSP5XXX.

Product Line:
Magelis HMIG5U/HMIG5U2, Pro-Face PFXSP5000 Series.

Resolution:
The Pro-face PFXSP5500XXX and PFXSP5xxx are equivalents to Schneider Electric's Magelis HMIDT and HMIGTU series (HMIG5U/HMIG5U2 or HMIG3U)

Please choose HMIDT according to the screen size you require as specified by PFXSP55000XXX. The options are HMIDT351, HMIDT542, HMIDT551, HMIDT642, HMIDT642, HMIDT732, HMIDT752, HMIDT952

Please choose between HMIG5U or HMIG3U as specified by the OS for PFXSP5xxx. The options are Windows Embedded Standard 7 SP1 for HMIG5U and VxWorks for HMIG3U.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: