Custom Engraved Legend Plates
Issue:
How do we order a custom legend plate?

Product Line:
Push Buttons and Operator Interface

Environment:
22mm and 30mm Push Buttons

Cause:
Product selection

Resolution:
Select which style, ie, plastic or metal, size, and color of legend plate you want. Order the special marking version of the legend plate part number and specify the marking desired with the order on the attached sheet.
.
Be careful not to exceed the maximum number of characters and lines available. See Digest or Push Button Specifier`s Guide for maximum numbers of characters and lines that are available for each legend plate.

Schneider Electric Việt Nam

Phần đính kèm
Copy of Nameplate.xlsx [392.71 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: