SFT2841 Setting and Operation Software Overview

Issue
Overview of the SFT2841 software for the SEPAM relay.

Product Line
SFT2841
SEPAM 20
SEPAM 40
SEPAM 80

Resolution
The SFT2841 software is the setting and operating tool for SEPAM series 20, SEPAM series 40 et SEPAM series 80. It may be used in 2 operating modes:
  • unconnected to SEPAM, to prepare parameter and protection settings
  • connected to SEPAM, to download and upload SEPAM parameter and protection settings and have access to all operating functions.
Please see attachment for more information.

Schneider Electric Việt Nam

Phần đính kèm

SFT2841 setting software.pdfSFT2841 setting software.pdf [266.91 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: