Can the ATV630 change the elaspe time reference in seconds be change to hours?
Issue:
ATV630 elaspe time reference configuration from seconds to hours

Product Line:
ATV630

Environment:
All serial numbers

Cause:
Customer request

Resolution:
No, the elaspe time reference in seconds can not to changed to hours. However it can be reset.
To do so:
Go to menu 4
Go to menu 4.8
Go to Time Counter Reset
Enter Run Time Reset

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: