Video: How to Configure Alarm Thresholds on your Symmetra PX10-80KVA UPS

Article available in these languages: Tiếng Tây Ban Nha

Issue:
How to Configure Alarm Thresholds on your Symmetra PX10-80KVA UPS using the integrated PowerView Display

Product line:
Symmetra PX1

Environment:
All Product models, all serial numbers

Cause:
Need for alerts when Load, Redundancy, or Runtime levels exceed predefined limits.

Resolution:
Select the Setup option from the main display
Select Alarms from the setup menu

The threshold you are setting is the minimum acceptable range. Changes are implemented immediately.

Hit escape to return to previous menu.

The following video demonstrates this procedure:

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: