How can I fix an error/warning message that reads that fonts are too small while working on SoMove?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Running SoMove and getting an error/warning message that fonts are too small

Product Line:
Altivar Altistart Tesys

Environment:
All

Resolution:
First try adjusting the fonts on your computer to a setting that works for you and for SoMove. If not possible, try the following;
... https://superuser.com/questions/1173048/some-applications-fonts-are-too-small/1261001
It's a Windows 10 issue, not a SoMove 2.6.3 issue
Note - I did have to right click first on the icon on the taskbar and then right click again on "SoMove" on the menu that pops up to get to the dialog box,
but the solution to go to the "Go to compatibility tab > Disable display scaling on high DPI settings" and restart SoMove worked.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: