How to combine horizontally / vertically 2 or more PrismaSeT G enclosures?
Prisma G enclosures can be combined in horizontal plan if they have the same height.
In the same way, in vertical plan PrismaSeT G enclosures can be combined if they have the same width.

Two enclosures are linked together with a combination kit. For more details please consult the PrismaSeT G catalog coded DESW025EN, available for download on www.schneider-electric.com).

Note: Enclosure extensions and ducts are delivered with 1 piece of LVS08815.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Phạm vi:
Tìm hiểu thêm
Sản phẩm:
Phạm vi: