What would cause the ATV630 Ethernet IP option card VW3A3720 to not show up in somove under the Fieldbus A slot?
Issue:
Causes for an ATV630 Ethernet IP option card VW3A3720 to not show up in somove under the Fieldbus A slot.

Product Line:
ATV630 with

Environment:
All

Cause:
ATV630 drives firmware is not at 1.5 or greater or you may need to build a project offline and then import the program into Somove.

Resolution:

Checked option 1 and it shows Ethernet IP card.  option 2 is no
Drive firmware is Version 1.5IEXX  or greater  which is good for the Ethernet IP option card.

Next Open up the Somove software:

Checked and we created a project offline adding the Ethernet IP card for option A

Now we copied the program from the drive and now it shows up as Ethernet IP under slot A in the Field bus section under Parameter list.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: