How to setup a run status on an ATS22 softstart?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
ATS22 run status setup

Product Line:
Altistart 22

Environment:
All

Cause:
Run status

Resolution:
Go into I/O menu.
Find R1 relay parameter.
R1 can be used as a run status.
R1 can be programmd to the following:
NSTP - starting - Relay is not energized at stop and is energized at all other times.
Run - running - Relay is energized when the bypass contactor is closed

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: