Varset and Reactivar capacitor banks environmental profile
Product line
Varset and Reactivar capacitor banks

Resolution

Our Low voltage capacitor banks are certified for  UL810, UL508a and CSA 22.2 190. There are no hazardous materials contained in any low voltage capacitor banks manufactured in the last 25 years. The products do not need any special end-of-life treatment. For more information on the individual capacitors, please refer to the attached documents according to the type:

1- M type in use since 1995 to 2004.
2-Varplus2 in use from 2004 to late 2011
3-VarplusCan in use since late 2011.


Schneider Electric Việt Nam

Phần đính kèm
M_cap_end_of_life_doc.pdf [311.7 KB]
Varplus2__end_of_life_doc.pdf [46.97 KB]
VarplusCan__end_of_life_doc.pdf [212.24 KB]