How does ZB5AFDA work?
The ZB5AFDA is looking like a selector switch but is in fact a push-push function locked in both positions with a key
Let's clarify (see attachment):
- This operator has 2 positions: 1 pushed on  and 1 pushed off.
- To change position, it is necessary to turn the key, push and turn back the key
- The product can be locked in both positions
- The key can be removed in both positions

Schneider Electric Việt Nam

Phần đính kèm
ZB5AFDA.pdf [59.04 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: