Tìm các câu hỏi thường gặp
What is the IK level for XAPM control station
The XAPM serie made of Zinc alloy (XAPM1*, XAPM2*, XAPM3*, XAPM4*) has been tested IK07 (according to EN 50102)
The XAPM serie made of Aluminium alloy (XAPM5*) has been tested IK06 (according to EN 50102)
For IK06, the energy is 1J
For IK07, the energy is 2J
The XAPM serie made of Aluminium alloy (XAPM5*) has been tested IK06 (according to EN 50102)
For IK06, the energy is 1J
For IK07, the energy is 2J
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: