Do Schneider products support the Large Forward Open in CIP communications
Issue
Ethernet/IP supported Frame format

Product Line
M580, M340, Quantum.

Environment
Unity Pro

Resolution
Schneider Products use Large Forward Open for Class 1 connections but only for CRAs. This type of connection is not available to other devices.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: