How can you read the PTH Power On Time status word parameter on the ATV660 drive over Ethernet?
Issue:
Reading the PTH Power On Time status word parameter on the ATV660 drive over Ethernet.

Product Line:
ATV660 and ATV960 drive

Environment:
All

Cause:
Wants to read the power on time PTH parameter in the input scanner map

Resolution:
You have to insert the PTH value in Somove using right click on the input table
and insert the PTH value. ( see the attachment file example).

Schneider Electric Việt Nam

Phần đính kèm
1CC36AE3AC93466C.jpg [101.11 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: