Tìm các câu hỏi thường gặp
What happens to the data points rtH, rtHI, and ptH on the ATV61 and ATV71 drives when it exceeds its maximum value of 65536 Hours?
Issue:
Data points rtH, rtHI, and ptH on the ATV61 and ATV71 drives exceed its maximum value of 65536 Hours
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Need to Reset Run time parameters after 7 years
Resolution:
When RTH, RTHI, PTH or PET value reaches 65535 (65535 hours = 2730 days = 7 years), the counter stays blocked at this value.
Also, It is impossible to reset PTH parameter.
Data points rtH, rtHI, and ptH on the ATV61 and ATV71 drives exceed its maximum value of 65536 Hours
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Need to Reset Run time parameters after 7 years
Resolution:
When RTH, RTHI, PTH or PET value reaches 65535 (65535 hours = 2730 days = 7 years), the counter stays blocked at this value.
Also, It is impossible to reset PTH parameter.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: