Video: How to configure the display network settings on a Galaxy VM

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Configuring Network Settings on Galaxy VM UPS Display

Product line:
Galaxy VM

Environment:
All Product models, all serial numbers

Cause:
How to configure the display network settings on a Galaxy VM

Resolution:
Go over the steps required to configure the network settings on a Galaxy VM.

The Galaxy VM comes equipped with a built-in network management card with the display, and has 2 empty SmartSlots for additional NMC if desired.  The Galaxy VM supports the AP9630, AP9631 and AP9635 SmartSlot cards only.

Start at the Home screen.
Select 'Configuration'

From the Configuration screen select 'Network' then 'Display' Make the changes needed to configure the network settings for the display.

The following video demonstrates this procedure:

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: