Is the MCS025 Sync-Check module compatible with the SEPAM 40 or 20 series?
Issue
Need to be able to check voltage from another source using the Sepam relay.

Product Line
Sepam 20
Sepam 40
Sepam 80

Environment
Digital relays

Resolution
The MCS025 Sync-Check module only works for the Sepam 80 Series.  It is not compatible with the Sepam 40 or 20 series.  For more information on the MCS025 module, please refer to FA221262.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: