Where can I find the pin diagram of the VW3A3725 Bacnet card?
Issue:
Where can I find the pin diagram of the VW3A3725 Bacnet card?

Product Line:
VW3A3725 Bacnet option card for ATV6xx series drives.

Environment:
All models, All serial numbers.

Cause:
N/A

Resolution:
This information can be found in the Altivar Process ATV600 Bacnet manual, document # QGH66984.02.   It is also listed below:

Schneider Electric Việt Nam

Phần đính kèm
Bacnet pinout.PNG.png [75.19 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: