Issue
What is the purpose of the F buttons on the Easergy P3 relay?
Product Line
Easergy P3
Resolution
F buttons are freely configurable for various purpose, both buttons are connected to an activation LED. Typical use of (but not limited to) the buttons:
What is the purpose of the F buttons on the Easergy P3 relay?
Product Line
Easergy P3
Resolution
F buttons are freely configurable for various purpose, both buttons are connected to an activation LED. Typical use of (but not limited to) the buttons:
- Control of an object
- Change setting group
- Activate/deactivate a function, e.g. auto recloser
- Reset latches
- Change or start/stop a programmable logic
Đã phát hành cho:Schneider Electric Việt Nam