How many EtheNet/IP adapters can be managed by LMC078?
There is no fix maximum of EtheNet/IP adapters managed by LMC078 as EtherNet/IP scanner (there is limit 16 on M251). Limit in LMC078 is given by the available load of the CPU, bus cycle task and the amount of transferred data.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: