Can both M580 redundant power supply modules provide the power at same time and equally
Question:
Can both M580 redundant power supply modules provide the power at same time and equally?

Answer:
No. M580 redundant CPS is designed to have only one active cps providing the power for the sake of life time difference. (or else, It is likely that both CPS fails around the same time which might cause the impact on the customer’s process)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: