RTC Synchronization with Time Zone over Internet in M172 performance controller
M17xP supports this BIBBS (Bacnet interoperability building blocks):
DM-TS-B(*) TimeSynchronization-B
so a Bacnet supervisor can synchronize it.

NTP (Network time protocol) is most common and widely used network protocol among the protocols used for clock synchronization of device over network
Today NTP / SNTP is not supported on M17xP controllers so it is not possible to synchronize the RTC of it to the NTP server.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: