The vertical cable manager is interfering with cage nut holes and the ability to mount equipment into the NetShelter cabinet, what's wrong?
Issue:
After installing finger-style cable managers the customer cannot install equipment.

Product Line:
AR7580A, AR7585, AR7588

Environment:
All serial numbers.

Cause:
The cable manager interferes with the mounting holes on the rails.

Resolution:
Intereference with the mounting holes on the rails is caused by one of two possible installation errors:

1) After attaching the cable manager to the rail the cable manager must slide towards the side of the cabinet, this will draw it away from the equipment mounting holes.
AR7580A - See installation step 6: https://www.apc.com/salestools/JKUR-948NBR/JKUR-948NBR_R1_EN.pdf
AR7585 - See installation step 6: https://www.apc.com/salestools/MLAN-8ZRM62/MLAN-8ZRM62_R1_EN.pdf
AR7588 - See installation step 6: https://www.apc.com/salestools/MLAN-8ZSRDH/MLAN-8ZSRDH_R1_EN.pdf

2) When installing the cable managers in the rear of a cabinet the accessory/PDU mounting rails must be moved out of the way. The cable managers cannot be installed atop the accessory/PDU mounting rails.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: