What type of cable can be connected to the A9XPCM04 connector?

To the A9XPCM04 it is possible to connect cable with the following characteristics:
- 35mm² max rigid wires (without ferrule)
- 25mm² max flexible wires (with ferrule)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: