Common mode filter for bearing current reductions for the ATV600 and ATV900 drives frame size three drives?
Issue:
Common mode filter for bearing current reductions for the ATV600 and ATV900 drives.

Product Line:
ATV600 and ATV900 drives frame size 3

Environment:
All

Cause:
Filter for bearing current reductions

Resolution:
The part number is VW3A5503 and its value of inductance is 120.0 uH

Schneider Electric Việt Nam

Phần đính kèm
Altivar Process ATV900_VW3A5503.pdf [93.46 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: