Are the ATV660 Zelio Smart Relays always programmed per the manual?
Issue:
Programming of ATV660 Zelio Smart Relays per the manual.

Product Line:
ATV660

Environment:
All

Cause:
Wiring

Resolution:

Per Seneca TAG, the Zelio program is the same as what's shown the manual, in all versions of Altivar660, unless there is something custom done on an order.  This would be a non-standard (i.e. not listed in the manual) modification.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: