Can a Surge suppressor be installed on the output of a variable speed drive?
Issue:
Can a Surge suppressor be installed on the output of a VFD?

Product Line:
ATV12, ATV312, ATV32, ATV320, ATV61, ATV71, ATV630, ATV930

Environment:
All

Cause:
NA

Resolution:
It is not recommended to put Surge Suppressor on load side of VFD. The PWM output of the VFD will damage the Surge Suppressor components.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: