What would cause the GV2AF4 adapter not to fit and connect to the ATV320 drive and the GV2 circuit breaker?
Issue:
GV2AF4 connection to ATV320 and GV2 circuit breaker.

Product Line:
ATV320 + GV2 breaker

Environment:
All

Cause:
GV2AF4 adapter pins are not long enough.

Resolution:
There is a newer adapter to connect the GV2 and the ATV320
The new part number is GV2AF5
There is a 29-day lead time on the part so you may need to contact customer service to see if you can expedite the order if needed.
The pins are longer to allow a better connection between the GV2 and the ATV320 drive.

Schneider Electric Việt Nam

Phần đính kèm
TeSys DF_ LS1-GK1_GV2AF5.pdf [69.87 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: