A customer is facing an issue with an XALE enclosure, bad outdoor resistance, is it normal ?These enclosures are declared IP54, "small rain", the best if you have an external application is to use the XALD range which is IP65.
Đã phát hành cho:Schneider Electric Việt Nam