Tìm các câu hỏi thường gặp
About Unica MGU3.701.xx keys
1) How many keys are delivered with the switch?
2 keys are delivered with each product.
2) Are these keys unique (for one device) or all of one series - same?
All products have the same key.
3) How and where is possible to order spare keys?
Keys are not delivered as spare parts.
4) Where can be removed the key? In which position?
You can remove the key only in 0 position.
Đã phát hành cho:Schneider Electric Việt Nam
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: