When using flange kits, what is the ATV630/930 depth dimension inside and outside the enclosure?
Issue:
ATV630/930 depth dimension inside and outside the enclosure when usinf a flange kit

Product Line:
ATV630 ATV930

Environment:
All mounted with flange kit

Cause:
Installation clearances

Resolution:
The flange kit allows the heatsink to protrude out the back of an enclosure. The VFD depth inside and outside of the enclosure is important for clearances.
See the attached file.

A is outside of enclosure
B is inside enclosure

Schneider Electric Việt Nam

Phần đính kèm
Dimension pictorial.pdf [51 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: