Video: Can I to create an array of structure in SoMachine V4.3 be exported to Vijeo Designer?
Yes, an array of structure created in SoMachine can be exported to Vijeo Designer.
First create a structure in SoMachine.  For an array of structure, create a regular array and select the structure name for the data type.
To export to SoMachine, right-click on the Symbol Configuration and select export to Vijeo Designer.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: