What does ramp increment mean for the Altivar Process drive?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Ramp increment meaning on the Altivar Process drive.

Product Line:
Altivar Process ATV600 ATV900

Environment:
All serial numbers

Cause:
N/A

Resolution:
Ramp increment is a parameter that will affect the resolution and the range of acceleration and deceleration parameters.
Inr [Ramp increment]
0.01 [0.01]: Ramp up to 99.99 seconds
0.1 [0.1]: Ramp up to 999.9 seconds
1 [1]: Ramp up to 6,000 seconds
This parameter is valid for [Acceleration] (ACC), [Deceleration] (dEC), [Acceleration 2] (AC2) and [Deceleration 2] (dE2).

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: