Where can I find documentation on ATV320 drives' physical dimensions?
Issue:
ATV320 dimensions request

Product Line:
Altivar 320, ATEV320 Altivar Machine

Environment:
All

Cause:
Need physical dimensions or drawings.

Resolution:
The best place to find the physical dimensions of any ATV320 drive is in the ATV320 Installation Manual, which can be found by following this link, or see the attached file.
https://www.se.com/ww/en/download/document/NVE41289/

Schneider Electric Việt Nam

Phần đính kèm
ATV320_installation_manual_EN_NVE41289_05.pdf [4 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: