Enclosed ATS22 soft starter is not running in Auto mode.

Article available in these languages: Tiếng Tây Ban Nha

Issue:
ATS22 Not Running in Auto Mode.

Product Line:
8639 22U enclosed ATS22

Environment:
All

Cause:
Auto start is not starting the soft starter.

Resolution:
Normally the auto start for auto is terminals 5-6.  So the end customer will need to close a set of dry contacts on these terminals to start the unit in Auto mode.

You can find the basic wiring diagrams in the Enclosed Altistart 22 manual
https://www.se.com/us/en/download/document/30072-453-26/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: