Why am I getting a digital signature error (Code 52) for the UNTLW WDM( Unitelway driver) Device in the Windows 10 Device Manger?
Issue:
Digital signature error (Code 52) for the UNTLW WDM( Unitelway driver) Device in the Windows 10 Device Manger


Product Line:
Unitelway driver


Resolution:
The Unitelway driver digital signature error (Code 52) occur because your current installed version of the Unitelway driver is not digitally signed for Windows 10. To resolve the issue, please install the latest version of the Unitelway driver. The latest version of the driver is 3.13 IE23. Please Click here to download the driver .

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: