​Information for Noise level of UPS Galaxy 5000 NAM
Issue:
Information for Noise level of UPS Galaxy 5000 NAM


Product line:
Galaxy 5000 NAM


Environment:
Galaxy 5000 40KVA, 50KVA,60KVA, 80KVA, 100KVA and 130KVA


Cause:
Customer needs UPS room noise level with Galaxy 5000.


Resolution: We publish this information. for Galaxy 5000.

Noise level
Measured according to ISO 3746 (NFS 31 027).
UPS acoustic pressure level for linear loads are indicated below.
UPS rating (kVA)40/50/60/80KVA100/130KVA
Noise level on a normal floor (dBA) with an RL load at 3 feet6563



Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: