Where can I find information on installing an ATV21 such as wiring, dimensions, etc.?
Issue:
Information regarding installation of ATV21.

Product Line:
Altivar 21

Environment:
All

Cause:
Need installation documentation

Resolution:
This information can be found in the ATV21 Quick Start Guide and the ATV21 Installation Manual.

The ATV21 Quick Start Guide can be downloaded from here:
https://www.se.com/ph/en/download/document/S1A73479/

The ATV21 Installation Manual can be downloaded from here:
https://www.se.com/au/en/download/document/AAV85581/

Both documents are also attached to this article.

Schneider Electric Việt Nam

Phần đính kèm
Altivar21QuickStartGuide.pdf [913.81 KB]
ATV21 Installation Manual 092009 AAV85581.pdf [1.79 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: