How do you wire an 8903L electrically held lighting contactor to a 3-wire photocell control?

Issue:
Wiring a 3-wire Photocell to an 8903L electrically held contactor

Product Line:
Lighting contactor

Environment:
8903 Type L electrically held

Resolution:
Most standard photocells have 3 wires.   Black is supply voltage, L1.  White is neutral or L2.  Red is the switched leg.   Run the switched leg to one side of the coil and the other side of the coil to the neutral or L2.   See attached diagram.

Schneider Electric Việt Nam

Phần đính kèm

Printing _8903 Electrically Held Type L Wiring Diagram - Form_ G10_.pdfPrinting _8903 Electrically Held Type L Wiring Diagram - Form_ G10_.pdf [7.95 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: