Video: How to read the data in the Profibus DP Diagnose of a PRM by M580?
Issue
How can I add a Profibus GSD file to Unity Pro library of Generic DTMs?

Product Line
M580, Unity Pro, PRM (TCSEGPA23F14F)

Environment
Unity Pro v13.0, STBNDP2212, M580, PRM

Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. This video will show you how to configure a Profibus slave (in this case a STBNDP2212) and read the data in the Profibus DP Diagnose Service using the PRM RDIAG function block.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: