Can PowerLogic Energy Meters (EMB and EME) monitor a 3-wire Delta system?

Issue
User wants to know if a PowerLogic Energy Meter (EMB and EME) can monitor a 3-wire Delta system

Product Line
PowerLogic Energy Meter (EMB and EME)

Environment
Wiring

Resolution
No, the PowerLogic Energy Meter (EMB and EME) cannot monitor a 3-wire Delta system.

PowerLogic Energy Meter (EMB and EME) can monitor the following systems:
1-phase, 2-wire
1-phase, 3-wire
4-wire Wye

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: