Can the ION meter template file be read before sending it to the meter?
Issue
Want to read the ION7650 template file before sending it to the meter

Product Line
Powerlogic ION meters

Environment
ION Setup
Text Editor

Resolution

The meter template file (DCF) is not human-readable and therefore cannot be read before sending it to the meter. When opened in a text editor like notepad, the file will display non standard characters.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: